Open a sample project
Open a sample project file to review the components and design of the provided application or layout.
To open a sample project:
- SelectSample Project.
- (optional) In theOpen Projectdialog box, select a file type from the list.
- Navigate to and select a sample project file.
- SelectOpen.
Provide Feedback