Create a new project from a sample project
Create a new project from a sample project to reuse the components in the new project.
To create a new project from a sample project:
- SelectFrom Sample Project.
- (optional) In theSelect Sample Projectdialog box, select a file type from the list.
- Navigate to and select a project file.
- SelectOpen. TheSave Asdialog box is displayed.
- In theNamebox, type a name for the new project file. The name is limited to 40 characters and must meet the IEC-61131 Name standard.
- (optional) In theLocation box, type or browse to a location to store the new project file.
- SelectSave.
Provide Feedback