Create a new Studio 5000 Architect project
Create a new
Studio 5000 Architect
project file to develop a layout for an automation system.A red outline around a box indicates that the value is invalid. Hover over the box to display a tooltip with additional information explaining why the entry is invalid.
To create a new
Studio 5000 Architect
project:- SelectNew Project.
- In theProject Typescolumn, selectArchitect.
- Select aArchitectproject template.
- Blank Projectcreates a new project with no components.
- Distributed Architecture - Multiple Process Serverscreates a new project with one engineering workstation and two Process Automation System Servers. Each PASS server controls five 1756ControlLogixcontrollers.
- Distributed Architecture - Single Process Servercreates a new project with one engineering workstation and one Process Automation System Server. The PASS server controls five 1756ControlLogixcontrollers.
- Process Skid with Logix Batch Sequence Managercreates a new project with onePanelView Plus 7graphic terminal that controls three 1769CompactLogixcontrollers.
- In theNamebox, enter a name for the new project. The name is limited to 40 characters and must meet the IEC-61131 Name standard.
- (optional) In theLocationbox, type or browse to a location to store the project file.
- SelectFinish.
Provide Feedback