Create a new project from an import

Create a new project from an import file to create a new
Logix Designer
project file based on an exported controller configuration (.l5k, .l5x, .xml).
To create a new project from an import:
  1. Select
    From Import
    .
  2. (optional) In the
    Select Project to Import
    dialog box, select a file type from the list.
  3. Navigate to and select a project file.
  4. Select
    Open
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal