Locate target modules using the Favorites tab
The
Favorites
tab in the Select Module Type
dialog box is similar to the Catalog
tab except there is not the option to Show Filters
or Hide Filters
. So there is no way to filter the module types based on their categories or vendors.- Start typing in the Search box to narrow the list of available modules in theFavoritesResults list.Only those module types that can be created under the given context display in the Favorites Results list, even though there might be more configured module types in the list. For example, some I/O Module types may have been added to Favorites. But when trying to configure module types under a 1769 backplane, the Favorites list would not show the I/O Module types because they are not valid under the 1769 backplane context.
- (optional) SelectClear Filterto start a new search.
- Select a module and selectCreateto configure module properties.
Provide Feedback