Change from a controller type in a different platform

When you change to a controller type within the same platform, the process deletes:
  • All non-default modules in the source controller (and their children)
  • All default modules in the source controller (and their children) that don't exist as default modules in the target controller; these are replaced by default modules for the target controller.
Module Input Data State Change
Changing from a controller that supports multiple event tasks configured to trigger on Module Input Data State Change to a CompactLogix 5370 L1 controller that only supports a single event task to trigger on Module Input Data State Change, preserves the configuration of the event tasks. A verification error is reported indicating that the module configuration is invalid. You must correct the error or change to a controller that supports this configuration.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal