PVLV status of permissives
Use the
General > Permissives
tab to monitor the status of permissives for the Process Valve (PVLV) instruction.To monitor the status of permissives for Process Valve (PVLV) instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Select theGeneral > Permissivestab.
- Monitor the status of bypassable and non-bypassable permissives for each state. A true (1) or false (0) indicator appears for each active permissive.
Provide Feedback