Configure the axis properties
After adding the drive and creating the axes, use the
Axis Properties
dialog box to configure and edit the axis properties for the drive. This dialog box is intended for an expert user who is accustomed to editing an axis.To configure the axis properties:
- In theController Organizer, expand theMotion Groupsfolder, and double-click the axis.
- Click the various pages of theAxis Propertiesdialog box to make the appropriate changes.Tip:Whenever there are pending edits on a tab, an asterisk (*) appears next to the page title to indicate pending edits.
- Click theApplybutton to save all the pending edits.If there are any errors detected, a message box appears indicating the error(s) and returns the focus to the field or item in question.
- ClickOKto close theAxis Propertiesdialog box, or clickCancelto reject all pending edits and close theAxis Propertiesdialog box.
Provide Feedback