Controller Organizer folders
The
Controller Organizer
window contains a hierarchical tree of the folders, files, and links that contain all of the information about the programs and data in the current project. For additional information about Controller Organizer
components, see:The table describes the folders that appear by default in the
Controller Organizer
directory structure.Folder | Description |
Controller Project Name | Contains controller-scoped tags, the controller fault handler, and the power up handler. |
Tasks | Contains tasks. Each task contains its own programs with routines (ladder, function block, sequential function chart, structured text), and program-scoped tags. |
Motion Groups | Contains groups of associated axes. Ungrouped Axes contains axes that have yet to be assigned to any axis group. You can assign these axes to specific motion groups with the Axis Assignment tab of the Motion Group Properties dialog box. |
Alarms | Contains tag-based alarms for tags and configured alarm definitions for Add-On Instructions and user-defined data types.
TIP:
Tag-based alarms are supported only on Compact GuardLogix 5380. CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, and GuardLogix 5580 controllers. |
Assets | Contains these project assets in sub-folders:
|
I/O Configuration | Contains the information about the hardware configuration of this controller project. It holds a hierarchy of modules with which the controller is configured to communicate. |
Provide Feedback