Restore window and toolbar defaults

You can, after rearranging your
Logix Designer
application, restore the factory default window and toolbar positions and sizes.
To restore window and toolbar defaults:
  1. On the main menu, select
    Window > Reset Window Layout
    .
  2. In the confirmation window, click
    Yes
    . The default layout of the
    Logix Designer
    application appears.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal