Bus Observer page
Use the settings on the
Bus Observer
page in the Axis Properties
dialog box to enable and configure the operation of the Bus Observer for a regenerative converter. The Bus Observer dynamically measures the active current applied to the DC Bus for the purpose of bus impedance compensation.
The
Bus Observer
page is available when, on the General
page, the Axis Configuration
is set to Regenerative AC/DC Converter
or Low Harmonic AC/DC Converter
and the Converter Configuration
is set to Bus Voltage Control
.
TIP:
To open the Bus Observer page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, clickGeneral.
- In theConverter Configurationbox, selectBus Voltage Control.
- InCategories, clickBus Observer.
The
Bus Observer
page includes these parameters.Parameter | Description |
|---|---|
Configuration | Determines the operation of the Bus Observer. Selecting Voltage Estimate configures the observer to dynamically estimate voltage based on an internal model of the DC Bus. This signal, when applied to the voltage loop, provides superior control loop performance. Use Voltage Estimate by itself or with the Bus Observer.The available values include:
This parameters are unavailable when in online mode and when the axis is Servo On . |
Bandwidth | Determines the proportional gain of the Bus Observer. The default value is 0.0 Hertz. This parameter is unavailable when Configuration is set to Disabled . |
Integrator Bandwidth | Determines the bandwidth of the integrator beyond which the integrator is ineffective. The default value is 0.0 Hertz. This parameter is unavailable when Configuration is set to Disabled . |
Provide Feedback