Publish multiple library objects
Multiple library objects can be published from an ACD repository at one time. Some objects may require additional information before they can be imported.
To publish multiple library objects from the ACD Repository to a folder repository or the ACM database
- Select multiple library objects.
- Hold down theShiftkey to select a contiguous block of library objects.
- Hold down theCtrlkey to select individual library objects that are not contiguous.
- Place the mouse within one of the selected items and drag all of the library objects on top of the folder repository or the ACM database. The Library Import Configuration window opens.IMPORTANT:When publishing into the ACM database the new library object will be compared to all library objects with the same catalog number that are currently stored in the ACM database, and many of the items in theLibrary Import Configurationdialog box will be completed using the information from the ACD or ACM database. Information that originates from the ACD cannot be edited in theLibrary Import Configurationdialog box.If publishing the library results in duplicated names, a warning message is displayed. ClickOKto proceed with publishing and accept the duplicate names.
- All of the selected library objects are listed under theNew Librariesheading.
- Select an item from the list to display its settings and enter the information for the library object.
- ClickOKonce all items have been entered to add all of the library objects at the same time.IMPORTANT:A red warning icon next to a library object in the list indicates that required information is not present for the library object.Library objects cannot be imported until all required settings are complete.If the required information cannot be supplied, clear the checkbox for that library object to omit it from the import list.
Provide Feedback