Unmount an ACD repository

While the ACD file is mounted in
Library Object Manager
, it cannot be opened in Logix Designer. When
Library Object Manager
is closed, the ACD file is automatically unmounted. However, to continue using
Library Object Manager
with other projects while editing an ACD file repository in Logix Designer, unmount the ACD file in
Library Object Manager
first.
To unmount an ACD repository
  • In the
    Library Repositories
    column, right-click the ACD repository and then select
    Unmount
    .
    The repository remains in the
    Library Repositories
    column, but the library objects are no longer accessible.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal