Add a folder repository

Library objects in the folder repository are organized according to a four-level hierarchy:
Solution -> Library Type -> Category -> Catalog Number(version number)
The catalog number and version number uniquely identify the library object. When ACM data is added to a repository, objects are displayed using this organizational method.
After adding the folder repository, add libraries and library objects.
To add a folder repository
  1. In the
    Library Repositories
    column, right-click
    Repositories
    then select
    Add Repository > Folder
    . The
    Browse For Folder
    window opens.
  2. Select a folder or create a folder.
    • Select a folder, and then click
      OK
      .
    • Click
      Make New Folder
      . A new folder is added to the current directory in the window. The name is highlighted. Change the name and click
      OK
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal