Apply substitutions to a symbol
Use substitutions to update elements of a symbol display.
To apply substitutions to a symbol
- After the symbol has been added, review the XML code in theSourcepanel of thePropertiescolumn.
- Highlight the item to be replaced, then right-click it and selectApply Substitution. TheSubstitution Builderdialog box opens with the highlighted text automatically placed in theOriginal Textbox.
- Click in theReplacementbox and enter the text to use instead of the original text. To use a calculated value as the replacement value, click the ellipsis (...) to open the Expression Builder window and create an expression.
- ClickOKto apply the substitution to the current symbol.The substitution is listed in theSubstitutionsfolder for use with other symbols.
Provide Feedback