Delete a trigger content
Delete a trigger content when it is no longer needed.
To delete a trigger content from a library object
- InLibrary Repositories, select the library object that includes the trigger content to delete.
- InLibrary Content, expand theME Alarmsfolder and theTriggerssubfolder.
- Right-click the trigger content and selectDelete.
- SelectYes.
Provide Feedback