Import an attachment
Import an attachment from an .HZ1 file to add it to an
Application Code Manager
database.To import an attachment from an .HZ1 file
- In, select Attachments.Library Object Manager
- SelectImport from .HZ1 Attachment Files.
- InImport HZ1 attachment file, browse and select one or more files, then clickOpen.
- (optional) If prompted, select whether to overwrite existing attachments in theApplication Code Managerdatabase.
- SelectingYesoverwrites attachment files. All files are imported.
- SelectingNocancels the import. No files are imported.
Provide Feedback