Tag CSV file format
If you want to put tags in folders, define the folders before you define the tags. The first section of the file contains the folder names. Use
F (for folder)
in the Tag Type
column and type the Folder name in the Tag Name
column. To put a tag in a folder, add the folder name to the tag name, and separate them with a backslash.The above use recommendations apply to importing databases. Databases for export should already be correctly formatted.
Tag file formats are the same for SE and ME.
Alarm file formats apply to SE applications only.
Provide Feedback