Tag Import and Export Wizard operations
In the
Tag Import and Export Wizard
dialog box, select the operation that you want to perform.Import & Export Choices | Description |
|---|---|
Export FactoryTalk View tag database to CSV files | Exports a FactoryTalk View tag database to CSV files. |
Import FactoryTalk View tag CSV files | Imports tag information from CSV files into a FactoryTalk View database. |
Export FactoryTalk View Client tags to CSV file | Exports client tags to a CSV file. |
Import FactoryTalk View Client tags CSV file | Imports client tags from a CSV file into a client computer. |
Merge FactoryTalk View tag database | Merges tag information from one FactoryTalk View project with another FactoryTalk View database. |
Import A.I. Series or Logic 5 database files | Imports symbols from the Rockwell Software A.I. Series, or Logic 5 CSV format into a FactoryTalk View database. |
Import RSLogix5/500 Address & Symbol ASCII files | Imports symbols from the ASCII export file of RSLogix5, or RSLogix 500 into a FactoryTalk View database. |
Provide Feedback