Merge FactoryTalk View tag databases

Use the Tag Import and Export Wizard to merge one
FactoryTalk View
tag database with another.
TIP:
The applications you select must be created on
FactoryTalk View
6.10 or later, or already converted to
FactoryTalk View
6.10 or later, otherwise the merging process will not succeed.
Project and database names must be unique on any one computer. Do not attempt to import a project to a location on the same computer (on a different drive, for example) that already has a project with the same name.
To merge
FactoryTalk View
tag databases
  1. In the first
    Tag Import and Export Wizard
    dialog box, select
    Merge
    FactoryTalk View
    tag database
    , and then click
    Next
    .
  2. Select the destination
    FactoryTalk View
    project. The
    Project
    type can be Machine Edition or Site Edition.
    1. Click the browse button to the right of the
      Project
      box to open the
      Select Destination Project
      window
    2. In the
      Select Destination Project
      window, navigate to the destination project's location.
    3. Select the project and click
      Open
      .
    4. Select the application development file (*.med or *.sed) and click
      Open
      .
  3. Click
    Next
    .
  4. Specify the import options and click
    Next
    .
  5. Verify the import information, and then click
    Finish
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal