Export FactoryTalk View client tags to a CSV file
Use the Tag Import and Export Wizard to export
FactoryTalk View
client tags to a CSV file.To export
FactoryTalk View
client tags to a CSV file- In the firstTag Import and Export Wizarddialog box, selectExport, and then clickFactoryTalk ViewClient tags to CSV fileNext.
- Specify the name of the application that you want to export client tags from.
- Select the destination file.In theSelect Destination Filesdialog box, you can accept the provided file name and path or change them as needed.
- ClickFinish.
Provide Feedback