Tag Import and Export Wizard
How do I open the Tag Import and Export Wizard?
Use one of the following methods:
- From WindowsStartmenu on the development system, selectAll apps > Rockwell Software > Tag Import and Export Wizard.
- InFactoryTalk View Studio, from theToolsmenu, selectTag Import and Export Wizard.
Use the Tag Import and Export Wizard to:
- Convert databases to and from a Comma Separated Variable (CSV) format compatible with Excel.
- Export the default client tags and import the customized tags.
- Merge oneFactoryTalk Viewtag database with another.
- Import an A.I.Series file, a Logic 5 text database file, or an RSLogix5/500 Address and Symbol ASCII file.TIP:The applications you select must be created onFactoryTalk View6.10 or later, or already converted toFactoryTalk View6.10 or later, otherwise the import, export, or merging processes will not succeed.Because ODBC data source names must be unique, project names on any given computer must be unique.
Provide Feedback