Log file parameters
The following table shows the log file parameters.
Parameter | Description |
|---|---|
x item(s) successful, x item(s) failed | Number of attempted replacements. |
Succeeded to replace | Name and location for item successfully replaced. |
Undo replacing | Name and location for replacement that was successfully undone. |
Failed to replace | Name and location that was not replaced. |
Unable to undo replacing | Name and location of item with changes that could not be undone. |
Provide Feedback