Find dialog box
How do I open the Find dialog box?
From the tool bar, click
, or select
, or select Find
from the Tools
menu.Use the
Find
dialog box to search for every occurrence of a specific tag, or text string in displays and global objects within FactoryTalk View
ME and FactoryTalk View
SE applications. Find
also locates all the text strings within each component that refer to the tag.Use the search and replace functions to search for and replace tags and text strings in the following product component types:
- Graphic Displays (does not include VBA)
- Global Objects (does not include VBA)
Provide Feedback