Create an Enable User button
Create an
Enable User
button to allow the administrator to enable a disabled FactoryTalk
user account from the current running application.To create an Enable User button
- In theGraphics Displayeditor, selectObjects > User Management > Enable Useror drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks.
Provide Feedback