Create an Add User/Group button
Create an
Add User/Group
button to allow the administrator to add a FactoryTalk
security user, a Windows-linked user, or a Windows-linked group to the current running application.To create an Add User/Group button
- In theGraphics Displayeditor, selectObjects > User Management > Add User/Groupor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks.
Provide Feedback