Create a Logout button
Create a
Logout
button to allow a logged in user to log out of the system at runtime.
TIP:
When a user logs out, the DEFAULT user is logged in.
To create a logout button
- In theGraphics Displayeditor, selectObjects > User Management > Logoutor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify the how the button looks.
Provide Feedback