Options on the Advanced tab of the Alarm Setup editor
The following table shows the options on the
Advanced
tab of the Alarm Setup
editor.Options | Descriptions |
|---|---|
Display | Select the graphic display used to show alarm messages. |
Current alarms | Click the Browse button (...) to select which graphic display is used to show alarm messages when an alarm is triggered. |
Edit | Click this button to open and modify the selected graphic display. |
Time settings | Specify notification hold time, maximum update rate, and embedded server update rate in this area. |
Hold time | Select the notification hold time (millisecond) to use when acknowledging, silencing, and resetting alarms. The application holds values at the Ack, Silence, Status Reset, and Close Display connections for the specified length of time, then resets the connections to zero. |
Maximum update rate | Select the maximum rate (second) at which data servers will supply data to the trigger tags specified on the Triggers tab. The default update rate is 1 second.This rate also applies to any tags used in trigger expressions, remote tags or expressions, and tags in trigger message embedded variables. At runtime, all of these tags are updated immediately upon startup, no matter what the update rate is. |
Embedded server update rate | Select the embedded server update rate (second) at which the data server will supply data to the tags in the trigger message embedded variables. The default update rate is set to match the alarm update rate. The embedded server update rate cannot be set to be larger than the maximum update rate. At runtime, all of these tags are updated immediately upon startup, no matter what the update rate is. |
History | Specify the alarm log file (.alm). |
Maximum number of alarm entries | Specify the maximum amount of alarm entries in the log file. The available value is 1-10,000. If the amount of alarm entries in the log file reaches the maximum capacity, the oldest alarm entry is deleted when new alarm occurs. |
Capacity high warning (%) | Specify the threshold of capacity high warning, which will occur when the amount of alarm entries reaches or exceeds the specified percentage of the Maximum number of alarm entries .The available value is 1-99. A write connection. Click the Browse button to assign a tag to the connection to notify the data source that the amount of alarm entries received has reached or exceeded the capacity high warning threshold. |
Capacity high-high warning (%) | Specify the threshold of capacity high-high warning, which will occur when the amount of alarm entries reaches or exceeds the specified percentage of the Maximum number of alarm entries .The available value is 1-99 and must be greater than the Capacity high warning value.A write connection. Click the Browse button to assign a tag to the connection to notify the data source that the amount of alarm entries received has reached or exceeded the capacity high-high warning threshold. |
Capacity overrun | Specify when the amount of alarm entries received exceeds the Maximum number of alarm entries and the oldest entry is overwritten.A write connection. Click the Browse button to assign a tag to this connection to notify the data source that the amount of alarm entries received has exceeded the Maximum number of alarm entries . |
Optional connections | Specify the following optional connections:
|
Name | This column shows the name of the connection. |
Tag or expression | Type the tag name or expression associated with the connection. If a tag or expression was selected, it is shown here. |
Tag button (...) | Click this button to open the Tag Browser and select a tag instead of typing the tag name in the Tag or expression column. |
Exprn button (...) | Click this button to open the Expression Editor and create an expression instead of typing the expression in the Tag or expression column. |
Provide Feedback