Options on the E-Signature tab of a graphic object's Properties dialog box
The following table shows the options on the
E-Signature
tab of a graphic object's Properties
dialog box.Options | Descriptions |
|---|---|
Require Electronic Signature | Select this check box to enable the electronic signature function. If this check box is clear, all other options on the E-Signature tab are disabled. |
Allow blank comment | If this check box is selected, the Comment box can be empty in the Electronic Signature window. |
Single Signatory | Configure the single signatory settings. |
Require re-authentication | If this check box is selected,password is required on the Operator tab in the Electronic Signature window.If this check box is clear, password is not required on the Operator tab in the Electronic Signature window. |
Counter Signatory | Configure the counter signatory settings. |
Require counter signature | If this check box is selected, all other options under the Counter Signatory settings are enabled. Authentication by another person is required to execute the action.If this check box is clear, all other options under the Counter Signatory settings are disabled. After the operator presses Accept in the Electronic Signature window, the action will be executed. |
Authorized Group | This list includes all the groups in FactoryTalk Security. If one group is selected from this list, all members of the selected group can be a supervisor of this object.You do not need to add the Authorized Group to Runtime Security. |
Domain Name | Configure the domain name for the Electronic Signature window. |
Visible | If this check box is selected, the options under the Domain Name settings are enabled, and the Domain button and box is visible in the Electronic Signature window.If this check box is clear, the options under the Domain Name settings are disabled, and the Domain button and box are invisible in the Electronic Signature window. |
Domain Name | Enter the domain name in this box. |
Variable Domain Name | Click the browse button to open the Tag Browser , and select a tag from the tag database for the domain name.Parameter is supported. |
Disable | If this check box is selected, the Domain button and box is disabled in the Electronic Signature window.If this check box is clear, the Domain button and box is enabled in the Electronic Signature window. |
Provide Feedback