CSV export status codes and messages
The following table shows the CSV export status codes and messages.
Status codes | Status messages | Descriptions |
|---|---|---|
0 | Not applicable | This is the initial status code value. |
100 | "Alarm information is being exported to a CSV file." "Audit information is being exported to a CSV file." "Diagnostics information is being exported to a CSV file." | Before the current export operation completes, you cannot perform another export operation. |
200 | "Alarm information has successfully been exported to a CSV file." "Audit information has successfully been exported to a CSV file." "Diagnostics information has successfully been exported to a CSV file." | The information is exported to a CSV file in the specified paths. |
700 | "Insufficient disk space to perform the export operation." | Delete files you no longer need from the disk you are saving to and export the information again. |
701 | "The path or address doesn't exist, or contains invalid characters." | Specify a valid path or address, or remove the invalid characters (\ / : * ? “ < > |), and export the information again. |
702 | "The file name contains invalid characters." | Remove the invalid characters (\ / : * ? “ < > |) and export the information again. |
703 | "The CSV file is missing." | Check whether the drive or address still exists and export the information again. |
704 | "Unknown error occurred.” | Export the information again. |
Provide Feedback