Options in the CSV Export Setup editor
The following table shows the options in the
CSV Export Setup
editor.Options | Descriptions |
|---|---|
Enable CSV Export | Select this check box to enable the options in the CSV Export Setup editor. |
Type | Select the type of information to be exported:
|
Path | Specify local paths to save the CSV files to. |
Connections | Specify tags or expressions for the connections:
|
Status | Specify tags for the selected information type:
|
Provide Feedback