Property Panel
How do I open the Property Panel?
When you open a project, the
Property Panel
is shown on the right in the main window. You can hide it, and change its size and position. If it is not shown, open it using one of the following methods:- On theGraphicstoolbar, click

- From theViewmenu, selectProperty Panel
- Right-click an object and selectProperty Panel
- Right-click an empty area of a display and selectProperty Panel
Use the
Property Panel
to modify the properties of graphic objects and assign tags and expressions to the objects. The Property Panel
is especially useful for making changes to the properties of multiple objects at the same time.Provide Feedback