Options on the Recipe tab of the RecipePlus Selector Properties dialog box

The following table shows the options on the
Recipe
tab of the
RecipePlus Selector Properties
dialog box.
Options
Descriptions
Column
Specify whether the selector will show a header, what the header text will be, and the column width.
Display header
Select this check box to show column headers on the object.
Select a column
Select a column to be edited:
  • Recipe.
    Shows the name of the recipe file.
  • Unit.
    Shows the name of the recipe unit associated with the recipe file.
Width
Type the width in pixels of the selected column.
Header text
Type the text to show for the header of the selected column.
List settings
Lines per item
From the drop-down list, select the number of lines each recipe/unit row will use in the selector. Range is from 1 to 10.
Word wrap
Select this check box if you want the text to continue on the next line at the beginning of a new word.
If this check box is cleared, the text continues on the next line whenever the maximum text length is reached, even if this occurs in the middle of a word or number. The maximum text length depends on the width of the object and the font size.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal