Columns on the Connections tab of a graphic object's Properties dialog box
The following table shows the columns on the
Connections
tab of a graphic object's Properties
dialog box.Columns | Descriptions |
|---|---|
Name | This column shows the name of the connection. |
Value update direction | This column shows an arrow to indicate in which way data can flow between the connection and the data source.
|
Tag/Expression | Type the tag name or expression associated with the connection. If a tag or expression was selected, it is shown here. |
Tag button (...) | Click this button to open the Tag Browser and select a tag instead of typing the tag name in the Tag/Expression column. |
Exprn button (...) | Click this button to open the Expression Editor and create an expression instead of typing the expression in the Tag/Expression column. |
Provide Feedback
connection updates the data source (write-only connection)
data source updates the connection (read-only connection)
connection updates the data source and data source updates the connection (read-write connection)