Create an ellipse or a circle object
Use the ellipse tool to draw ellipses and circles.
To create an ellipse or a circle object
- In theGraphics Displayeditor, selectObjects > Drawing > Ellipseor drag
from the toolbox. - Press the mouse button, drag the mouse diagonally to draw the object to the desired size, and release the button.PressCtrlas you drag the mouse to draw a circle
- Double-click the object to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how you want the object to look.
- ClickOK.TIP:Because of a limitation in the Windows CE operating system, ellipses or circles that look fine on the desktop may appear ragged when shown on the PanelView Plus family terminals. To avoid this, do not use ellipses with a line width greater than 1 pixel.
Provide Feedback