Options on the General tab of the Image Properties dialog box
The following table shows the options on the
General
tab of the Image Properties
dialog box.Options | Descriptions |
|---|---|
Image | Enter the file name of the graphic image or click the Browse button to select the file name in the Image Browser . The image appears on the face of the object, to show the information about what the object does.Before you can place an image on the object, you must import the image into the project. |
Image back style | This property applies to monochrome and color images. Use it to set the background style to Solid or Transparent .If Image back style is Transparent :
|
Image color | This property applies to monochrome images. It determines the color the image is drawn in; that is, the foreground color. Click the colored box to select another color. |
Image back color | This property applies to monochrome images. It determines the color of the background the image is drawn on. Click the colored box to select another color. If the Image back style is Transparent , the background of the image will be transparent. |
Image blink | Select this check box to let the monochrome image blink at runtime. The image blinks twice per second. |
Provide Feedback