Create an arc object
Use the arc tool to draw arcs. The arc shape is a segment of an ellipse's perimeter. To create an arc, you first draw an ellipse or circle, and then edit it to form an arc.
To create an arc object
- In theGraphics Displayeditor, selectObjects > Drawing > Arcor drag
from the toolbox. - Press the mouse button and drag the mouse diagonally to draw an ellipse the size you want.When you release the mouse button, a set of handles appears so you can reshape the ellipse.TIP:PressCtrlas you drag the mouse to base the arc on a circle.
- Grab a handle and drag the mouse to change the size of the arc.To grab a handle, point the mouse cursor at it and when the arrow changes to a cross-hair cursor, click the left mouse button.
- Double-click the arc to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how you want the arc to look.
- ClickOK.TIP:
- If you apply rotation animation to an arc object, when the display is run on aPanelView Plusfamily terminal, the arc may change to an ellipse at one point in the rotation, but does not affect the arc's function.
- Because of a limitation in the Windows CE operating system, arcs that look fine on the desktop may appear ragged when shown on aPanelView Plusfamily terminal. To avoid this, do not use arcs with a line width greater than 1 pixel.
Provide Feedback