Create a text object
Use the text tool to draw a text object to use for labels or instructions on the display.
To create a text object
- In theGraphics Displayeditor, selectObjects > Drawing > Textor drag
from the toolbox. - Press the mouse button, drag the mouse diagonally to draw the object to the desired size, and release the button.TheText Propertiesdialog box opens.
- Enter the text and specify the options.TIP:
- To move the cursor to the next line of text, pressEnter.
- To use an embedded variable in the text, clickInsert Variable.
- To create another text object, move to an empty spot in the drawing area, click and drag to create another text object.
- ClickOK.
Provide Feedback