Create a panel object
Use the panel tool to draw rectangles and squares that have borders. You can set up panel objects to blink at runtime. The panel object only supports visibility animation.
To create a panel object
- In theGraphics Displayeditor, selectObjects>Drawing > Panelor drag
from the toolbox. - Press the mouse button, drag the mouse diagonally to draw the object to the desired size, and release the button.TIP:PressCtrlas you drag the mouse to draw a square panel.
- Double-click the panel to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how you want the panel to look.
- ClickOK.
Provide Feedback