Create a freehand object
Use the freehand tool to draw shapes as you would with a pen on paper.
To create a freehand object
- In theGraphics Displayeditor, selectObjects>Drawing > Freehandor drag
from the toolbox. - Press the mouse button, drag the mouse diagonally to draw the object to the desired size, and release the button.
- Double-click the object to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how you want the object to look.
- ClickOK.
Provide Feedback