Options on the Audit tab of the Audit Trail List Properties dialog box
The following table shows the options on the
Audit
tab of the Audit Trail List Properties
dialog box.Options | Descriptions |
|---|---|
Columns | Specify which columns to use, their time and date format, and what header text they will show, if any. |
Display header | Select this check box to show column headers on the object. |
Select a column | Select a column to be edited:
|
Display column | Select this check box if you want the selected column to appear on the object. |
Time and date format | Select the time and date format to show. The available options reflect the settings in your development computer’s operating system. In Windows, these are found in the Regional and Language options in the Control Panel . If the operating system settings are different on your development and runtime systems, the runtime settings are used at runtime.This option is available only when Occurred Time is selected. |
Header text | Type the text to show for the header of the selected column. |
Column width | Define the width of the selected column in pixels. This option applies only to the Source , Location , Resource , and Username columns. |
List settings | Specify the amount of lines each audit can use and word wrap behavior for messages. |
Lines per audit | Select the number of lines, from 1 to 10, each audit will occupy in the list. |
Word wrap | Select this check box if you want the text to continue on the next line at the beginning of a new word. If this check box is cleared, the text continues on the next line whenever the maximum text length is reached, even if this occurs in the middle of a word or number. The maximum text length depends on the width of the object and the font size. |
Provide Feedback