Options on the Alarm tab of the Alarm List Properties dialog box
The following table shows the options on the
Alarm
tab of the Alarm List Properties
dialog box.Options | Descriptions |
|---|---|
Columns | Specify which columns to use, the symbols to show, if any, their time and date format and what header text they will show, if any. |
Display header | Select this check box to show column headers on the object. |
Select a column | Select a column to be edited:
|
Display column | Select this check box if you want the selected column to appear on the object. |
Time and date format | Select the time and date format to show. The available options reflect the settings in your development computer’s operating system. In Windows, these are found in the Regional and Language options in the Control Panel . If the operating system settings are different on your development and runtime systems, the runtime settings are used at runtime.If the Acknowledge Symbol , Active symbol , or Message column is selected, this option is unavailable. |
Header text | Type the text to show for the header of the selected column. |
Symbol | Type a symbol to show beside an acknowledged or active alarm. |
List settings | Select how many lines each alarm can use, how selected alarms will be indicated, and word wrap behavior for messages. |
Lines per alarm | Select the number of lines, from 1 to 10, each alarm will occupy in the object. The default is 1. |
Selected alarm indicator | Select whether the selected alarms will be indicated by a highlight bar or by a cursor. |
Word wrap | Select this check box if you want the text to continue on the next line at the beginning of a new word. If this check box is cleared, the text continues on the next line whenever the maximum text length is reached, even if this occurs in the middle of a word or number. The maximum text length depends on the width of the object and the font size. |
Filtering | Filter the object to show only the alarms from the specified triggers. |
Filtered triggers | Click the Browse button to open the Trigger Label Selector, where you can select the alarm trigger labels whose alarms will be included on the display as they occur.If this box is blank, all alarms are shown. |
Provide Feedback