Options on the Display tab of the Alarm List Properties dialog box
The following table shows the options on the
Display
tab of the Alarm List Properties
dialog box.Options | Descriptions |
|---|---|
Alarm conditions | Alarms can be acknowledged or unacknowledged, active or inactive. Specify the conditions for the alarms that will be displayed in the alarm list at runtime. |
Select alarm condition | Select an alarm condition from the list. |
Active and acknowledged | Select this item and the Display check box to show the alarms that are active and acknowledged. |
Active and unacknowledged | Select this item and the Display check box to show the alarms that are active but not acknowledged. |
Inactive and acknowledged | Select this item and the Display check box to show the alarms that are no longer active but are acknowledged. |
Inactive and unacknowledged | Select this item and the Display check box to show the alarms that are no longer active and have not been acknowledged. |
Display | Select this check box to show the alarms that match the selected alarm condition at runtime. |
Blink | Select this check box if you want the alarms that match the selected alarm condition to blink at runtime. |
Use alarm colors | Select this check box if you want the alarms that match the selected alarm condition to be shown using the colors specified in the Alarm Setup editor.If this check box is cleared, alarms will be shown using the colors specified in the Back color and Fore color boxes. |
Back color | This box shows the current background color for the alarms matching the selected alarm condition. Click the box to select a different color. |
Fore color | This box shows the current color of the shown text for the alarms matching the selected alarm condition. Click the box to select another color. |
Provide Feedback