Create a Shutdown button
At runtime, the operator can use the
Shutdown
button to shut down the application. When the operator presses the button, the application closes, stopping all project components, and returns to Windows.To create a Shutdown button
- In theGraphics Displayeditor, selectObjects > Advanced > Shutdownor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks.
Provide Feedback