Create a scale
Use the scale object to draw a line with tick marks on it.
The scale can be used as a ruler or measuring guide. For example, you can place the scale next to a bar graph, with text labels at the top and bottom, to illustrate the range of the bar graph.
To draw a scale
- In theGraphics Displayeditor, selectObjects > Gauge and Graph > Scaleor drag
from the toolbox. - Press theMousebutton and drag the mouse diagonally to draw the scale.
- When the scale is the desired size, release the button.
- Double-click the scale to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the scale looks.
Provide Feedback