Create a Return to Display button
At runtime, the operator can press a
Return to Display
button to close the graphic display that the button is on and reopen the display that was previously open.To create a Return to Display button
- In theGraphics Displayeditor, selectObjects > Display Navigation > Return Toor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks.
Provide Feedback