Create a Ramp button
At runtime, the operator can use the Ramp button to increase or decrease the value of a tag. Ramp buttons can change a value by either an integer or floating point value. You can use two Ramp buttons together to create a raise/lower control.
TIP:
Configure a numeric display object to show the value of the Ramp button’s Value connection.
To create a Ramp button
- In theGraphics Displayeditor, selectObjects > Push Button > Rampor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify the how the button looks, its tags, and whether to use auto repeat.
Provide Feedback