Create a numeric display
Use the numeric display object to show the operator numeric information from the data source. For example, you might use a numeric display to show the current temperature of an oven in a bakery.
To create a numeric display
- In theGraphics Displayeditor, selectObjects > Numeric and String > Numeric Displayor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the display to be.
- Double-click the display to open itsPropertiesdialog box.
Provide Feedback