Options on the Timing tab of the Multistate Push Button Properties dialog box
The following table shows the options on the
Timing
tab of the Multistate Push Button Properties
dialog box.Options | Descriptions |
|---|---|
Auto repeat settings | |
Auto repeat rate | Select the number of times per second a button press is registered when the button goes into auto repeat mode. Select 0 if you don’t want to use auto repeat. |
Auto repeat delay | Select the length of time the button has to be pressed and held down before auto repeat starts. |
Provide Feedback