Create a Macro button
The
Macro
button runs a specified macro when the operator presses it at runtime.To create a Macro button
- In theGraphics Displayeditor, selectObjects > Advanced > Macroor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks and what macro will run when it is pressed.
Provide Feedback